Portable Handle Spacer

IMPORTANT SAFETY NOTICE Generac Power Systems, Inc. re-announces recall of certain 2013-2021 Portable Generators Generac® XT8000E, XT8000EFI, GP6500, GP6500E, GP8000E, HomeLink 6500E and DR® PRO 6500M and PRO 6500E. If you responded to the initial recall and received a handle guard kit, we have you on the list to receive a free spacer repair kit and no further action is necessary on your part at this time. If you own a Generac portable generator that is included in the safety recall and did not receive the previous kit, please continue to “Get Started” and provide the needed information.

Redeem

Generac Reannounces Recall of Portable Generators; Additional Finger Amputation and Crushing Injury Reported; New Repair Kit Available

Release Date: November 10, 2022
Recall Number: 23-040

Recall Summary

Name of Product: Generac® and DR® 6500 Watt and 8000 Watt portable generators

Hazard: An unlocked handle can pinch consumers' fingers against the generator frame when the generator is moved, posing finger amputation and crushing hazards.

Remedy: Repair

Consumers should immediately stop using the recalled portable generators, unless the locking pin has been inserted to secure the handle in place before and after moving the generator, and contact Generac for a free repair kit consisting of a set of spacers to move the handle away from the frame, eliminating the pinch point. Customers who had responded to the original recall will automatically be sent a new kit.

Consumer Contact:

Generac toll-free at 844-242-3493 from 8 a.m. to 5 p.m. CT Monday through Friday, or online at www.generac.com/handlespacer or www.generac.com and click on Important Safety Information for more information.

Recall Details

Units: About 321,160 (In addition, 4,575 were sold in Canada) These portable generators were previously recalled in July 2021.

Description: This recall involves 6500-watt and 8000-watt Generac portable generators with unit type numbers XT8000E XT8000EFI, GP6500, GP6500E, GP8000E and HomeLink 6500E portable generators, and DR models PRO 6500M and PRO 6500E portable generators. This recall also involves all of these generators listed above purchased after July 29, 2021 through November 3, 2022, containing a repair kit which included full cover handle guards. The generators have gasoline-powered engines that are used to generate electricity for use as backup power. The portable generators have two-wheels and a single, U-shaped, two-grip, flip-up pin-lock handle to help move the generator. Only the following generators are included in this recall. The unit type is identified on the front of the product. The model and serial numbers are printed on a label on the product. Consumers can also check specific unit type, model number, and serial number location information at www.generac.com/service-support/product-support-lookup

Handle Spacer Unit type graph

Incidents/Injuries: The firm has received a total of 37 reports of injuries, 24 resulting in finger amputations and five in finger crushing.

Sold at: Major home improvement and hardware stores nationwide and online, including Ace Hardware, Amazon, Blain's Farm & Fleet, City Electric Supply, Costco, Do it Best, Fastenal, Home Depot, Lowe's Stores, Napa Auto Parts, Northern Tool & Equipment, Orgill, Power Equipment Direct, Ravitsky Bros., True Value, and W.W. Grainger from June 2013 through June 2021 for between $790 and $1,480.

Manufacturer: Generac Power Systems, of Waukesha, Wisconsin

Manufactured in: United States and China

Note: Health Canada's press release is available at: recalls-rappels.canada.ca/en/alert-recall/generac-and-dr-portable-generators-recalled-due-finger-amputation-and-crush-hazards

Photos

Recalled XT8000E Generator

Recalled XT8000E Generator

Recalled XT8000EFI Generator

Recalled XT8000EFI Generator

Recalled GP6500 Generator

Recalled GP6500 Generator

 

Recalled GP6500E Generator

Recalled GP6500E Generator

 

Recalled GP8000E Generator

GP8000E

 

Recalled PRO 6500M Generator

Recalled PRO 6500M Generator

Recalled PRO 6500E Generator

Recalled PRO 6500E Generator

Recalled Homelink 6500E Generator

Recalled Homelink 6500E Generator

About the U.S. CPSC
The U.S. Consumer Product Safety Commission (CPSC) is charged with protecting the public from unreasonable risk of injury or death associated with the use of thousands of types of consumer products. Deaths, injuries, and property damage from consumer product-related incidents cost the nation more than $1 trillion annually. CPSC's work to ensure the safety of consumer products has contributed to a decline in the rate of injuries associated with consumer products over the past 50 years.

Federal law prohibits any person from selling products subject to a Commission ordered recall or a voluntary recall undertaken in consultation with the CPSC.

For lifesaving information: